AXIS#.IL.PWMQUIET

Description

0 - Operate at nominal PWM modulation frequency only. The nominal frequency limits power consumption, but results in acoustic noise.

1 - Automatic control of PWM modulation frequency. Operate at maximum frequency, outside the audible range, when allowable, to eliminate acoustic noise.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

0 to 1

Default Value

1

Data Type

Integer

See Also

AXIS#.IL.KP

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.IL.PWMQUIET

500ah

17h

Unsigned8

-

-

Read/Write

No

AXIS2.IL.PWMQUIET

510ah

17h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.IL.PWMQUIET

5828

16C4

Unsigned8

Read/Write

-

AXIS2.IL.PWMQUIET

71364

116C

Unsigned8

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.IL.PWMQUIET

5828

Unsigned8

Read/Write

-

Related Topics

"Current Loop"